SIMATIC Visualization (SiVArc)

Support of standardized connections – independent of the platform

Challenge

Standardize the user interfaces across the plant for improved visualizations, created with significantly reduced engineering efforts

 

SiVArc

Solution

Automatic generation and creation of visualizations based on the program code of the controller and corresponding visualization objects as part of comprehensive library concepts

 

Technical features

  • Integration in the TIA Portal starting with V14

  • Controller support: S7-1200, S7-1500, ET200SP

  • HMI support: Basic Panels, Comfort Panels, and Mobile Panels 2nd generation

  • PC-based support: WinCC Runtime Advanced, WinCC Runtime Professional, S7-1500 software controller

  • SiVArc is configured using rules (not programmed!)

 

Added value

  • Automatic creation of visualizations – drastic reduction in engineering time!

  • Reduced commissioning times by prevention of errors at an early stage

  • Adaptation of the visualizations based on modifications/adjustments in the control program at the touch of a button