![]()
|
PortfolioFor more than a hundred years Siemens Marine Technology has been specializing in the design, manufacture and commissioning of electrical equipment for all types of merchant vessels, naval vessels and submarines worldwide. Our automation systems and diesel-electric drive systems are installed in a large number of vessels. In times of intensified environmental awareness Siemens Marine Solutions is readily prepared for Green Ship Solutions featuring low emission electric propulsion systems including waste heat recovery. Siemens also specializes in turnkey projects and conversions. Our subsidiaries are located throughout the world and offer service and after sales support. A long history of successSiemens first venture onto water was in 1874, when its English subsidiary, Siemens Brothers, operated a special ship called the FARADAY to lay transatlantic cables between Europe and America. In order to avoid having to stop work at night, an electrical system was installed on the Faraday in 1877, the first in the world on a ship. The equipment consisted of a direct current generator and a large arc lamp. This lamp contained two carbon electrodes to which voltage was applied until a bright arc light was created between them. It thus became possible to completely light up the deck of the Faraday.One year later, Siemens launched the differential arc lamp on the market, in which the carbon rods, which gradually burned away, were re-adjusted automatically. It was therefore possible to connect several lamps to one generator and use them to illuminate the ship. The arc technique was more suitable for projector lights but it was the best kind of lamp at the time, given that gas lighting on ships was not a possibility. In 1879, Siemens equipped three German ships with electrical installations: the HANNOVER, the THEBEN and the HOLSATIA were fitted out with generators, projector lights and interior lighting. In the same year, Siemens and Halske delivered a power generation and lighting system to England for the steam ship CITY OF BERLIN. These orders more than 125 years ago are regarded as the official start of a long history of success: Siemens had boarded and was to remain on board ship. |
||