Membrane Bioreactor (MBR) Systems
Biological Wastewater Treatment
Wastewater Clarification
Anaerobic Digestion Products
Chemical Feed and Disinfection
Wastewater Odor Control Systems
Chicago, Illinois, USA, Oct 20, 2008
For the trade press
Siemens Water Technologies is adding the new Sludge Belt Dryer to its array of sludge dewatering options. This convective dryer is supplied in a one- or two-belt design that provides uniform evaporation and has an adjustable speed belt to vary residence times. System advantages include efficient operation in minimal space, low emissions, low dust, a granular final product and a low thermal requirement with possible heat recovery from low temperature waste energy sources. By making better use of wastewater solids and waste heat, communities can lower their energy costs, helping to save space in landfills and encouraging the recycling of nutrient-rich wastewater solids.

Sludge Belt Dryer from Siemens Water Technologies
In the Sludge Belt Dryer, evaporation takes place when the biosolids come in contact with the heated air. The sludge is uniformly distributed on the entire belt width to cause uniform evaporation. Evaporative capacities are 1,000 to 13,000 pounds (454 to 5,897 kg) of water evaporated per hour, and the system is designed to operate continuously if required. The mechanically dewatered feed material can be handled within a wide range of moisture contents, which in most cases exceed the range of other dryer types. With a heat requirement of approximately 1,441 BTU/lb (less than 800 kcal/kg) of evaporated water, the dryer allows for great heating flexibility. The ability to vary residence times in the drying zone provides a way to fine tune the product moisture to meet final use or disposal requirements. The dryer can also be fitted with a product cooling zone when needed. The Sludge Belt Dryer will be featured at WEFTEC.08 in Booth # 28077, Hall B. Further information about solutions for water treatment available at http://www.siemens.com/water A photo supplements this press release. Please see: http://www.industry.siemens.com/data/presse/pics/IIS200810354.jpg
The Siemens Industry Sector (Erlangen, Germany) is the world's leading supplier of production, transportation and building systems. Integrated hardware and software technologies combined with comprehensive industry-specific solutions enable Siemens to enhance the productivity and efficiency of its customers in industry and infrastructure. The Sector comprises six Divisions: Building Technologies, Industry Automation, Industry Solutions, Mobility, Drive Technologies and Osram. In fiscal 2007 (ended September 30), Siemens Industry generated sales of approximately EUR40 billion (pro forma, unconsolidated) with around 209,000 employees worldwide. http://www.siemens.com/industry With the business activities of Siemens VAI Metal Technologies, (Linz, Austria), Siemens Water Technologies (Warrendale, Pa., U.S.A.), and Industry Technologies, (Erlangen, Germany), the Siemens Industry Solutions Division (Erlangen, Germany) is one of the world's leading solution and service providers for industrial and infrastructure facilities. Using its own products, systems and process technologies, Industry Solutions develops and builds plants for end customers, commissions them and provides support during their entire life cycle. Further information and downloads at: http://www.siemens.com/industry-solutions
Wieland Simon
wieland.simon@siemens.com
Phone: +49 (9131) 7-46169
Fax: +49 (9131) 7-25074
www.siemens.com/industry-solutions
Search for more press releases