Membrane Bioreactor (MBR) Systems
Biological Wastewater Treatment
Wastewater Clarification
Anaerobic Digestion Products
Chemical Feed and Disinfection
Wastewater Odor Control Systems
Drive technology for the water industry
Drive technology is absolutely decisive when it comes to
the availability and efficiency of pumping stations and
blowers in the water industry. Here, Siemens offers
harmonized and coordinated drive solutions for all
applications in the water/wastewater sector – from just
a few Kilowatts up to 30 Megawatts.
They optimize the reliability and quality of the water
supply and water treatment plants using precise
processes and maximum availability. At the same time,
they guarantee low operating costs and a high degree of
cost-effectiveness.
Equipment used in water supply and wastewater treatment
plants must often run for long periods of time without
any interruption or even continuously. Our motors
increase the availability of the complete system thanks
to their rugged design, long service lifetime as well as
low maintenance and reliable operation. For instance,
our Durignit insulation system for low-voltage motors
and Micalastic for high-voltage motors guarantee
excellent protection against corona discharge, make our
motors and generators insensitive to environmental
effects - ensuring the highest service lifetimes and
endurance.
This is complemented by bearing and winding monitoring
devices that are included as standard.
An additional positive feature: The compactness. Our
motors set standards when it comes to power-related
envelope dimensions and weight. This saves space and
makes it easier to integrate motors into the overall
plant or system.
High degrees of efficiency improve the energy balance
therefore reducing operating costs. Low noise and low
vibration levels complement all of these features.
Siemens low-voltage and high-voltage motors fulfill all
of the requirements in the water business – both fresh
and wastewater.
Especially for pump drives that are typical used in
water supply and water treatment plants, or blower
compressors for stabilizing ponds, variable-speed
operation using a drive converter saves a
considerable amount of energy, makes processes more
flexible and therefore reduces the stressing on the
complete plant or system. Thanks to these cost
savings, the pay-back time for a frequency converter
drive is often just a few months.
The cost-saving potential and pay-back time of such
an investment can be quickly and simply calculated
using our SinaSave energy-saving program. Using
plant-specific data, such as flow rate, delivery
head, pumping profile over a day and over a year,
working shifts and working days etc., SinaSave
determines the energy demand of variable-speed
systems compared to alternative concepts. These
alternative concepts include various types of
closed-loop throttle controls, bypass systems or
pole-changing motors. The program calculates the
pay-back time from the purchase price of the
appropriate drive converter, the energy saving based
on the actual cost of energy and other additional
cost-reducing factors associated with variable-speed
drives. These factors include, for example, the
elimination of mechanical controls, lower stressing
on the overall system and a higher overall
efficiency.
With traditional control techniques, the motor always runs with the speed designed for the maximum pumped quantity and the excess quantity is throttled using mechanical actuator elements. When all is said and done this means that the energy is simply wasted. On the other hand, with converter-based drive systems, the speed is adapted to the actual operational requirements and therefore also the amount of energy drawn. In other words – the motor only draws the power that is precisely necessary at that particular operating point. In this case, power factor and efficiency remain almost constant over a wide range. By changing the speed, the pump characteristic is shifted to an optimum for the specific process. The overall result is a significantly lower energy demand than for fixed-speed drives with the same power rating that use mechanical control principles in the partial load range. The energy-saving effect is especially high for pumps, fans, compressors and blowers. The reason for this is that in this case the power drawn is proportional to the speed to the power of three. Even slight speed changes result in a considerable energy saving effect. Depending on the plant or system characteristic, the energy saving as a whole can be up to 50% - whereby for steep system characteristics, the energy saving potential is especially high.
When current peaks are eliminated this also
eliminates the associated torque surges – that can
be quite significant. The soft starting and stopping
reduces the stressing on the complete mechanical
transmission line as well as the piping system and
increases its lifetime.
In addition to the soft starting and stopping that
reduces the stress on the system, variable-speed
operation avoids unfavorable operating conditions
such as cavitation, gas being pumped along with the
medium, compression surges and vibration that can
also damage the plant. Partial load eddy effects and
the associated eddy losses are eliminated.
Additional advantages of frequency converter
operation include the fact that mechanical controls
are eliminated, the power factor is improved as well
as the closed-loop process control that is optimized
when compared to mechanical principles.
When using variable-speed drives, the flow rate can be controlled far more accurately with short response times than when applying mechanical control concepts such as throttles. Even for brief fluctuations in the water demand or the amount of wastewater, the pump system can more quickly and more precisely adapt the pumped quantity to the actual requirement. This results in a higher degree of reliability and quality in water supply and wastewater treatment plants.
Siemens drive converters, such as the SINAMICS G150 and MICROMASTER units and SIMOVERT MV for medium voltage, have a concept that is designed to very effectively utilize the energy-saving potential. These drive converters have been specifically designed for drive applications without regenerative feedback into the line supply – especially for pumps, fans and blowers.