Basic PLC Functionalities

More functionality at no extra charge

With the aid of the basic PLC functionality (free function blocks) integrated as standard in the SINAMICS G inverters, simple logical and arithmetic operations can be created directly in the inverter. Processing is reproducible and irrespective of the PLC cycle time.


Application examples:

Rapid traverse / creep speed switchover and Quick Stop depending on a light barrier.

 

This is an integrated function of the following frequency inverters: