Tools

Site ExplorerSite Explorer
Close site explorer

Programming variables for cycles

Using R parameters

Manufacturing several variants of workpieces is often required. To do that, different parts programs are usually created with different values. A simpler approach is to use R parameters or variables instead of program values. An additional benefit to be gained from programming variables is that the parameters can be reconciled and combined using mathematical functions.

The SINUMERIK Operate user interface makes implementing this complex programming even easier. This is true for the programming with programGuide as well as for ShopTurn and ShopMill. As shown in the “Groove” illustration, the values are replaced by parameters. These must be specified at the beginning of the program or can be loaded by another program. For example, a start program is created for machining that covers the different variants of the group of parts.

Example

The parameters are specified directly in the program, just as in the image, or over an initial setup program.

Example for combining variables

IF R20 = R10+2/(R5*3,1419)
R15=25
ENDIF
MSG(“MAXIMUM DIAMETER REACHED”)