CNC4you Worldwide

Site Search

Menuclose
Related
Info
close
Programming counter-spindlesin G-code

Programming counter-spindles
in G-code

Programming counter-spindles in G-code

Counter-spindle

Standard lathes have a spindle into which the workpiece is chucked and then machined with turning or milling tools. To allow the workpiece to be completely machined (including the “back” side) it must be rechucked by hand – a process in which errors can often be made at the expense of the precision of the workpiece. By using machines with counter-spindles, this process is automated, allowing a much higher level of precision to be achieved. These counter-spindles pick off the workpiece from the main spindle with positional accuracy so that it can be completely machined on one machine. The operator can simply program takeover of the workpiece with ShopTurn in one cycle. If ShopTurn is not available, synchronization must be programmed via G-code.


Programming example

The following example describes this sequence. Siemens accepts no liability for the general validity and functional safety of the program example shown.

Text

Synchronous takeover at 1000 rpm

COUPDEF(S3,S1,1,1,“NOC“,“DV“)

; S3 is counter-spindle

COUPON(S3,S1)

; S1 is main spindle

G95 S1000 M4

Handover

M?

; Open M-function to counter-spindle chuck with spindle rotating

G0 Z2=300

; Preliminary position of counter-spindle absolute dimension

G94 G1 Z2=280 F1000

; Pick-off position absolute dimension approach at 1000 mm/min

G4 F0.5

; Dwell time

M?

; Close M-function to counter-spindle chuck with spindle rotating

G4 F0.5

; Dwell time

M?

; Close M-function to main spindle chuck with spindle rotating

G4 F0.5

; Dwell time

G0 Z2=600

; Pull-back position counter-spindle absolute dimension

Pull-back position counter-spindle absolute

COUPOF(S3,S1)
COUPDEL(S3,S1)
M1=5
M3=5

MIRROR Z0

; Mirror the machining, programming in Z minus direction

SETMS(3)

; Select master spindle for counter-spindle

Note:
With the mirror command, the control system automatically resets the path correction commands (G41/G42 and/or G42/G41) in keeping with the change in machining direction – that is, G42 external machining is also programmed on the counter-spindle.

Machining on the counter-spindle

G55

; Zero point of counter-spindle

MIRROR
M30

; Deselect mirroring


You are changing from the tablet to the classic version. Do you want to proceed?