Coordinate Cube

Swiveling accurately

"Know exactly what is required." Finally, extensive considerations for determining the coordinate axes and the sign for the direction of rotation are no longer necessary. The coordinate cube consists of a single piece of material. The coordinate axes can either be labeled separately or be engraved directly in the milling machine. The cube is an informative example for the simple use of the CYCLE800 swivel cycle.


Note

The programs and files have been created and tested with the greatest care in accordance with the requirements listed in the manufacturing description. However, the manufacturing of the workpieces offered is at your own risk. Siemens accepts no liability for damage to property or personal injury. Workpiece manufacture is only permitted for private and not industrial use. Passing on the manufactured workpieces or production documents to a third party for commercial gain is strictly prohibited.