Multiple technologies allow Siemens to offer the most efficient odor control solution
The Ministry selected Siemens for its odor control experience and number of installations in the Kingdom. Siemens is one of the few bidding companies that was able to provide a multitude of odor control solutions, including a combination of biological, chemical, and activated carbon. Siemens will also guarantee the overall system’s efficiency.
Two two-stage bio-trickling filters will remove the bulk of hydrogen sulfide (H2S) in the aerated grit chambers and bio-phosphorus tanks, followed by a LO/PRO two-stage chemical scrubber to reduce overall odors. A three-stage chemical scrubber will remove 99.9% of H2S and other odors in the sludge thickener and tanks area. Three additional scrubbers will be installed in the sludge dewatering building to treat ammonia and amines, H2S, and organic sulfur compounds in three separate stages. A ZABOCS biofiltration unit installed in the return and excess sludge pumping station will remove H2S and various other odorous compounds. A single-stage packed tower chemical scrubber in the aeration tanks rounds out the system, treating a high volume of air and a range of odors and concentrations in a small footprint.
For this project, Siemens again teamed up with Riyadh-headquartered project manager Aziz.
Siemens Water Technologies has a number of odor control installations in the Kingdom of Saudi Arabia, including a chemical scrubber in Wady Al Dawasir; six carbon systems in Riyadh; seven biological systems and four carbon systems in Dhahran; and two biological systems in Taif.
Further information about solutions for water treatment is available at http://www.siemens.com/water
A photo supplements this press release. Please see:
http://www.industry.siemens.com/data/presse/pics/IIS200910843.jpg