Sep 24, 2001 | The exact time for process synchronization by satellite - Siclock now with IRIG interfacesSiclock TS, the plant clock from the Siemens Industrial Solutions and Services Group (I&S), now has integrated interfaces based on the US standard, IRIG (Inter-Range Instrumentation Group). At the output of the plant clock, there are IRIG A signals or IRIG B signals to choose from. In addition, Siclock TS can be synchronized with IRIG A or IRIG B signals on the input side. The new interfaces reduce the effort and expense of planning, testing and commissioning. The clock receives signals by satellite via the Global Positioning System (GPS). more |
Sep 24, 2001 | Simit as an engineering station for Simatic PCS 7 – Siemens simulation tool now with new interfaces and linksThe Simit simulation system is now linked to the Simatic PCS 7 process control system as well as having extended interfaces to Profibus and OPC. The range of applications of this tool from the Industrial Solutions and Services Group (I&S) of Siemens extends from a pure offline simulator for the design phase up to the real-time simulation of complex systems in combination with automation equipment. Simit thus becomes the engineering station for the PCS 7 process control system. Without any additional hardware, the complete "virtual system" can be simulated for all systems at the field level and automation level right up to operator stations on the screen of a single computer. This enables errors to be detected and eliminated at the configuring stage, thus saving configuring costs and simplifying commissioning. more |
Sep 07, 2001 | Aida-IX/net facilitates the administration of Unix-based networksWith its new software tool Aida-IX/net, the Electronic Design House of the Industrial Solutions & Services Group (I&S) of Siemens simplifies automatic installation, documentation and administration of Unix-based networks. more |
Aug 09, 2001 | Siemens to supply plant and equipment for a new papermaking machine for Rhein Papier GmbH in HürthThe Siemens Industrial Solutions and Services Group (I&S) has received an order from Rhein Papier GmbH - part of the Myllykoski Corporation of Helsinki, Finland - to supply automation and electrical equipment of the latest design for the PM 1 papermaking machine being installed in the company's new paper mill in Hürth. At the heart of the installation is an integrated process automation system based on Simatic PCS 7 process control. The order is worth around EUR 15 million and also includes all the power distribution equipment and drives. Commissioning of the new papermaking machine is scheduled for the summer of 2002. more |
Jun 25, 2001 | Quality management at the most modern level of international standardization - Siemens I&S receives certification in compliance with ISO 9001The Siemens Industrial Solutions and Services (I&S) Group is the first group in Siemens AG to receive direct certification in compliance with the new quality standard DIN EN ISO 9001:2000. The quality management system for the entire I&S portfolio for industry and infrastructure, covering the complete plant life cycle, was audited and certified. Fulfilling the broadened ISO 9001 standard guarantees that the group is able to provide solutions and services which satisfy customer requirements as well as official regulations. more |
Jun 25, 2001 | New standard for factory-wide automation with Simatic PCS7 - Siemens offers universal automation solution for the paper-making industryWith its solution concept based on the process control system Simatic PCS7 Siemens Pulp and Paper Technologies offers the paper and pulp industry a universal and comprehensive automation solution for the entire factory. In addition to the production lines it also allows auxiliary plants such as power plant, fresh-water services, clarification plant and packaging plant to be monitored and controlled. All important information are always readily available across the company. Operator control and monitoring are facilitated with a uniform user interface for all processes. Standard software modules for the MES and process control level as well as for quality management ensure universal data flow between process and production planing. A simulation model supports project planning and commissioning of new plant and refurbishments. Thus the new standard systems for the paper-making industry help from planning through to running production to reduce costs, increase system availability and ensure adherence to environment and quality standards. more |
Jun 20, 2001 | Safe and efficient earth testing with the Siemens Geowid B4156 - A new method allows single earths to be measured in meshed and interlinked earthing systemsThe Geowid B4156 Tester from the Siemens Industrial Solutions and Services (I&S) Group is intended for the safe and efficient measurement of the earthing in meshed or interlinked systems. A new method of measurement using split-core-type current transformers allows the selective testing of earthing arrangements without the use of spikes and without having to disconnect individual branches. It allows parts of electrical systems to be tested while they are still in operation and regardless of any parallel earthing. Individual lightning-protection conductors, such as those on HV towers, can also be measured. more |
Jun 20, 2001 | Standard safety for electrical equipment - Siemens appliance testers offer total fully-automatic testing in accordance with DIN VDE standardsThe new B4130 and B4131 protective safety testers from the Siemens Industrial Solutions and Services (I&S) Group are able to test electrical equipment and appliances in accordance with the requirements of the very latest standards. They are microprocessor-controlled and provide total testing in accordance with the most recent edition of DIN VDE 701-1:09.2000 and repeat testing in accordance with DIN VDE 0105 and DIN VDE 0702. This means that it is a simple matter to ensure that appliances and equipment are safe to use after they have been serviced, repaired or modified. more |
May 31, 2001 | Ulrich Gerdemann is appointed President of Siemens Industrial ServicesWith effect from May 1, 2001 Ulrich Gerdemann (55) has assumed the Presidency of the Industrial Services (IS) Division of the Industrial Solutions and Services (I&S) Group of Siemens AG. With around 21,000 employees throughout the world, IS is one of the leading providers of technical services in the sectors of industry, energy and infrastructure. Ulrich Gerdemann was previously responsible for the Infrastructure and Marine Solutions (IMS) Division of I&S. more |
May 30, 2001 | Modern process control system increases production capacity - Siemens integrates automation and drive technology in a French paper factoryThe Industrial Solutions and Services Group (I&S) of Siemens AG has been awarded a contract by Papeteries Etienne S.A., Arles, France, to modernize the electrical equipment for two paper machines and a winder. The production lines will be equipped with a PCS 7 process control system and a new drive controller. This modernization will participate to improve substantially the production capacity of the factory. The value of the contract is over 2 millions EUR. Commissioning of the modernized facility is planned for the end of 2001. more |