siemens.com
Português
Home | Processes | Products, Solutions & Services | News | References | About us
Site Map | Contact Us
Upstream
Midstream
Downstream


 
Home > Processes > Midstream > LNG Production

GT-LNG | E-LNG
 

GT-LNG — Better Solutions

Next-generation LNG plants will be designed to achieve an annual output of 6 to 8 million tons or more, requiring upwards of 240 MW of total compressor power for the refrigeration process alone. As a result, compressors and their respective drivers will be considerably largerscale compared to today’s installed base. Tomorrow’s plants, however, won’t just be built around larger machines, but better solutions.

Siemens has introduced its renowned SGT6-2000E (ex V84.2, 110 MW (ISO) at 3,600 rpm) and SGT5-2000E (ex V94.2, 160 MW (ISO) at 3,000 rpm) as LNG mechanical drive gas turbines. These units not only exceed currently available products in their respective class by approximately 20% in power rating. They are also optimized for maximum periods between inspections and shortest maintenance downtimes, requiring just four days of maintenance after 16,000 equivalent operating hours (EOH) and 16 days after 48,000 EOH. This is, in part, due to the silo combustors at each side of the gas turbine casing, which can be accessed by a normal-sized person for inside inspection. What’s more, the SGT6-2000E and SGT5-2000E can handle both low calorific fuel gas and gas with a high content of nitrogen.

With a track record of more than 220 installations, these gas turbines have proven their credibility in generator drive applications around the world — applications which are typically more demanding than continuous-load LNG operation.

For small-size refrigeration trains, Siemens offers the well-proven SGT-600 and SGT-700 mechanical drives, rated ISO 25.5 MW and 30 MW respectively.
     

 

 

 

     
 

 © Siemens AG 2008 - Oil & Gas
Corporate Information / Privacy Policy / Terms of Use / Digital ID