siemens.com
Português
Home | Processes | Products, Solutions & Services | News | References | About us
Site Map | Contact Us
Upstream
Midstream
Downstream


 
Home > Processes > Midstream > LNG Production > E-LNG > Power generation

Water-steam cycles | Gas turbines | Steam turbines | Synchronous generators | Power transmission and distribution | Stability
 

Power generation - Stability

Power systems for E-LNG plants exhibit an unusually low ratio of generating capacity to single electrical loads. Typically, the power consumption of some very large motors is distributed over a few generators, resulting in a low CAPEX and a highly reliable system. The main challenge is to maintain a stable power-system frequency under all circumstances. Stability in this context is essentially defined as keeping the power-system frequency within the limits set by the gas-turbine speeds.
 

Siemens’ superimposed electrical network monitoring and control computer (ENMC) monitors all major electrical loads in order to keep the power-system frequency stable.
  The Siemens E-LNG concept is based on an n+1 powerplant design: All gas and steam turbines in service operate permanently at part load, and the n-units assume full load within a very short time in the event of an unexpected shutdown of the surplus turbogenerator. Redistributing the load onto the operational turbogenerators is a key to liquefaction- compressor stability.
 

Understanding the stability challenge

In-house simulation tools allow Siemens to accurately predict and document the stability of the E-LNG power system under single-fault conditions, within specified environmental and operating conditions, and fuel supplied to the power plant according to agreed parameters. Electronic variable speed drive systems (VSDS) employed to drive the main refrigerant compressors can function as negative spinning reserve in the power rebalancing process; they can reduce their speed (and thus their power consumption) instantaneously upon the unexpected loss of a turbogenerator in the power plant. The amount of negative reserve is determined by the momentary compressor stability line.

Siemens’ stability solution is based on the following principal functions: fast signal and data exchange between all control and protection systems of the power-to-compression system; intelligent use of positive and negative spinning load reserves; modified gas-turbine IGV controls, pre-control systems; and a dedicated superimposed electrical network monitoring and control system (ENMC, patent pending).
 

Mitigating side effects

Electronic VSDS are non-linear electrical loads on the electrical system. As such they can exhibit side effects in the form of power-line harmonics, inter-harmonics, oscillating torques in the drive motors, and possible electromagnetic interferences (EMC) throughout the electrical system. Siemens has developed effective mitigation measures for all these unwanted effects. Passive harmonic filters are custom-engineered for each project. The effects of interharmonics are simulated, and corrections in control strategies are implemented if necessary. Oscillating torques in motor-compressor strings are damped sufficiently by design measures and rotor inertia. Effects of active and passive electromagnetic interferences on the entire electrical distribution system are investigated and solutions developed at the Siemens EMC research center, the largest of its kind in Europe.
 

Ensuring quality from component to system level

Full lateral and torsional analyses according to international standards are performed in-house and documented for each rotating string prior to detail design. API vibration criteria and tests are generally applied to motor-compressor strings. Electrical stability of the power system, load-flow and short-circuit calculations, protection coordination, and load-shedding scenarios based on specified emergency shut-down (ESD) actions are routinely determined by our system engineers and made available to our clients and their consultants.
     

 

 

 

     
 

 © Siemens AG 2008 - Oil & Gas
Corporate Information / Privacy Policy / Terms of Use / Digital ID