siemens.com
Português
Home | Processes | Products, Solutions & Services | News | References | About us
Site Map | Contact Us
Upstream
Midstream
Downstream


 
Home > Processes > Midstream > LNG Production > E-LNG > Power generation

Water-steam cycles | Gas turbines | Steam turbines | Synchronous generators | Power transmission and distribution | Stability
 

Power generation

For any E-LNG scheme, power-plant availability is key. Operated under island-type conditions without the possibility to export or import electricity, Siemens’ expertise and experience as the leading OEM supplier of turnkey power plants worldwide makes all the difference in ensuring ultimate reliability.

LNG plants are typically located remotely from populated areas, frequently without access to stable and robust powertransmission networks. As a result, power stations for E-LNG plants operating in island mode have to meet special requirements, including self-controlled system frequency with fast response capability, steep load gradients, and tolerance for harmonics. Specifically, measures have to be implemented to ensure a fast transfer of electric loads within such island power systems to keep the liquefaction process running within specifications. Only then, the core benefit of five years or more of uninterrupted service offered by the E-LNG design concept can be fully leveraged.

Air cooled standardized combined-cycle power plants in modular construction are cost effective, environmentally friendly and highly reliable generating facilities for E-LNG plants.


Combined-cycle schemes for optimum efficiency

An initial decision for operators and investors to make is choosing the type of power plant and the method of financing and building it. Self-cooled combined-cycle power plants are the proven state-of-the-art solution, outperforming simple-cycle power plants with about 40 percent higher thermal efficiency and a 30 percent reduction in greenhouse-gas emissions. They consist of gas turbines, waste-heat recovery boilers, and steam turbines to make maximum use of the feed gas, and reduce emissions. Building such power stations in accordance to the manufacturer’s standardized modular design results in cost effective projects and yields maximum value for owners and investors. While Siemens delivers simple-cycle power plants as well, combined-cycle schemes are recommended for their superior performance.
 

Combined-cycle schemes for optimum efficiency

An initial decision for operators and investors to make is choosing the type of power plant and the method of financing and building it. Self-cooled combined-cycle power plants are the proven state-of-the-art solution, outperforming simple-cycle power plants with about 40 percent higher thermal efficiency and a 30 percent reduction in greenhouse-gas emissions. They consist of gas turbines, waste-heat recovery boilers, and steam turbines to make maximum use of the feed gas, and reduce emissions. Building such power stations in accordance to the manufacturer’s standardized modular design results in cost effective projects and yields maximum value for owners and investors. While Siemens delivers simple-cycle power plants as well, combined-cycle schemes are recommended for their superior performance.
 

Ensuring continuous productivity

In order to guarantee uninterrupted supply of electricity even during unscheduled outages of turbogenerators, surplus generation capacity has to be installed in the power plant and operated at all times. Following the so-called n+1 principle, an additional turbogenerator provides the positive spinning reserve that prevents temporary overloading of generators in the event of one unit failing. In the E-LNG concept, all turbines and generators operate continuously in part-load, capable of assuming full load in a very short time, without affecting the power output or the refrigeration process. The cost of the additional generator is easily compensated through additional 15+ productive days per year an E-LNG plant achieves compared to traditional gas-turbine driven plants. However, if an adequate powergrid connection is available at or near the project site, the n+1 generator may be omitted.
 

Adapted to specific E-LNG power plant needs

Gas turbines are typically designed for maximum efficiency, meaning maximum firing temperatures. In order to optimize the whole economic model of an LNG plant taking into account the importance of availability, the gas turbines are adapted and operated at lower firing temperatures. This allows the operator to achieve exceptionally long maintenance intervals up to six years for a major overhaul while having fast load reserve available during operation.
 

Financing tailored to customer needs

Siemens’ standardized power-plant designs are modular and expandable, pre-engineered to a large extent, and make use of local content wherever appropriate. These designs are easily and cost-effectively integrated into E-LNG plant projects. Independent power-producer (IPP) concepts are available for alternative financing schemes of such power plants, removing CAPEX from the project balance sheet and paying power-consumption charges from the OPEX budget instead.  
 

Related Links

References
Power Generation


 

 

 

     
 

 © Siemens AG 2008 - Oil & Gas
Corporate Information / Privacy Policy / Terms of Use / Digital ID