siemens.com
Português
Home | Processes | Products, Solutions & Services | News | References | About us
Site Map | Contact Us
Upstream
Midstream
Downstream


 
Home > Processes > Downstream > Gas-to-Liquids (GTL)

Air Separation, Air Compression | Refining | Utilities | Power Generation Island
 

Air Separation, Air Compression

Determining the achievable economies of scale, air separation or air compression are the single most important parts of any GTL plant. It is here where the world’s largest compressors are employed. Depending on the applied process, they feed massive volumes of air either directly to the gas reforming stage, or to a cryogenic separation process, which provides oxygen for the conversion of natural gas into syngas.

Siemens’ latest very-high-volume STC-SR main air compressor represents a significant step towards the economies of scale required from air separation plants for tomorrow’s GTL schemes. Delivering an amazing 700,000 cubic meters of air per hour, it effectively surpasses first-generation machines while retaining maximum long-term reliability.

Next-generation GTL plants, however, will employ even more powerful compression solutions. In order to keep the required number of compressor trains within reasonable limits, future main air compressors will have to achieve a volume flow of 900,000+ cubic meters per hour — corresponding to an air separation unit output of 5,000+ tonnes per day of oxygen. At Siemens, these compressors are part of a continuous development program designed to meet the growing demand of megascale applications. Moreover, before being shipped and installed at customers’ sites, even the largest of these compressor trains — encompassing main and booster air compressor, and a double-ended condensing steam turbine — will have passed string-testing at Siemens’ unique large-scale compressor test bed.
     

Compression

Very-high-volume main air compressor
Booster air compressor


Drives

Electric motors
Steam turbines
Gas turbines

Related Links

References

     

 

 

 

     
 

 © Siemens AG 2008 - Oil & Gas
Corporate Information / Privacy Policy / Terms of Use / Digital ID