siemens.com
Português
Home | Processes | Products, Solutions & Services | News | References | About us
Site Map | Contact Us
Press Releases
Fairs & Events
Technical Reports


 

For the trade press

Siemens installs demineralization line for OMV refinery in Burghausen, Germany

Erlangen, 2007-06-25
 

The Siemens Industrial Solutions and Services Group (I&S) is installing a new demineralization line in the Burghausen refinery for OMV Deutschland GmbH and connecting it to existing systems. This aim is to cover the boiler feedwater needs of the expanded ethylene plant. Commissioning of the demineralization line is scheduled for summer 2007.


The OMV refinery in Burghausen. Here, Siemens is installing a new demineralization line for the expanded ethylene plant (photo source: OMV).
  OMV Deutschland GmbH is the leading mineral-oil company in south Germany. With a 45 % holding in Bayernoil Raffineriegesellschaft, OMV has an annual crude-oil refining capacity of 8.8 million metric tons. The refinery in Burghausen mainly produces high-quality middle distillates, petrochemical raw materials and petroleum coke for the aluminum industry.

With the commissioning of the new cracking furnaces of the expanded ethylene, the need for boiler feedwater has increased. This necessitates a third treatment line (Row 6) for fully demineralized water from well water and a second mixed bed filter. The process engineering and technical aspects of the new line will be such that it will reliably produce salt-free potable water that can be used for high-pressure steam boilers.

Siemens is to build the complete demineralization line and integrate it into the existing systems. The new line includes a cation and anion exchanger – each of which uses a fluidized bed procedure and has a capacity of 180 m³/h – plus CO2 removal by means of a trickler, including blower, and also pumping with trickle pumps, one of which will be in operating mode and the other in stand-by mode. The mixed bed exchanger with a capacity of 360 m³/h is also part of the scope of supply. In addition, the media needed for operating the demineralization line such as compressed air, hydrochloric acid and caustic soda will be integrated into the existing plant and into the supply and removal systems.

Siemens is also responsible for planning, designing, project management, manufacturing and commissioning as well as trial operation and preparation of the documentation.

Further information on products, systems, solutions and services for the oil and gas industry at: www.siemens.com/oil-gas  

A photograph supplements this press release. Please see:
www.industry.siemens.com/data/presse/pics/07065497.jpg  

The Siemens Industrial Solutions and Services Group (I&S) is the integrator of systems and solutions for industrial and infrastructure facilities and global service provider for the plant and projects business covering planning, installation, operation and the entire life cycle. I&S uses its own products and systems and process technologies in order to enhance productivity and improve competitiveness of companies in the sectors of metallurgy, water treatment, pulp and paper, oil and gas, marine engineering, open-cast mining, airport logistics, postal automation, intelligent traffic systems and industrial services. In fiscal 2006 (to September 30) I&S employed a total of 36,200 people worldwide and achieved total sales of EUR 8.819 billion, according to U.S. GAAP.

Further information and downloads at: http://www.industry.siemens.com

 
Reference number: I&S 0706.5497 e
Press Office Industrial Solutions and Services
Dr. Rainer Schulze
Tel.: +49 (9131) 7-445 44
Fax: +49 (9131) 7-25074
E-mail: rainer.schulze@siemens.com


back

 
 

 © Siemens AG 2008 - Oil & Gas
Corporate Information / Privacy Policy / Terms of Use / Digital ID