siemens.com
Português
Home | Processes | Products, Solutions & Services | News | References | About us
Site Map | Contact Us
Onshore
Offshore - Drilling
Offshore - Production
Pipeline - Compressor and Pumping Station
Pipeline - Valve, Metering, Custody Transfer Station
Pipeline - Main Control Centere, Sub-Control Center
Pipeline - Infrastructure
LNG - Production
E-LNG - Electric drive solutions
E-LNG - Compressors
E-LNG - Power generation
LNG - Terminals
Terminal Management and Automation
Refinery
Olefins
GTL / CTL
Utilities
Power Generation Island
Test-Bed Facility


 

E-LNG - Electric drive solutions - Statoil, Hammerfest

One of two liquefaction compressor drivers rated 65 MW at 3600 rpm for the Statoil Snøhvit project in Hammerfest (Norway). These LCI-supplied 2-pole brushless synchronous motors are complemented by a 32 MW/3600 rpm and one 16 MW/6600 rpm motor, all of which have been full-load full-speed tested prior to shipment to the site.

Additional Siemens scope of supply: 
VSDS-driven compressor string for the methane mix train;
32-MW VSDS for the liquefication compressor;
CO2 re-injection compressor;
harmonic study;
containerized load-commutated inverter (LCI) frequency converter units, drive control and fault diagnosis systems;
transformers;
containerized harmonic filters;
converter cooling systems and auxiliary equipment.
     

E-LNG - Electric drive solutions - NAM, Groningen

One of three motor-driven natural-gas compressors rated 38 MW/4200 rpm at NAM’s UGS facility near Groningen, Netherlands. Operational since 1986, these machines were the largest VSDS at that speed until the Hammerfest drives were built in 2004.

Additional Siemens scope of supply: 
entire electrical system from 150 kV power supply to medium and low-voltage distribution;
harmonic filters, including installation and commissioning;
LTSA for the drive systems.
     

E-LNG - Electric drive solutions - NAM, Groningen

One of NAM’s compressor stations producing natural gas from the Groningen gas field in the Netherlands. A series of 16 (ultimately 21) motor-driven depletion compressor sets rated 23 MW at 6100 rpm have been supplied since 2001, the world’s first electrical high-speed variable-speed drive systems in that class with active magnetic bearings.

Additional Siemens scope of supply: 
harmonic filter plant and all auxiliaries;
fan motors for cooling banks;
system integration; 
conceptual and detail engineering; 
network analysis and vibration studies.
     

E-LNG - Electric drive solutions - North Africa

Two starter/helper motors rated 17 MW at 3600 rpm supply starting power and additional torque for the gas turbines at an LNG plant in North Africa. A total of eight such 2nd-generation variable-speed drive systems have been ordered for mechanically driven LNG refrigeration compression systems since 2003, using 2-pole solid-steel turbo-rotor motors with brushless excitation and LCI-type variable-frequency drives.
     

E-LNG - Electric drive solutions - STEAG, Germany

Two boiler feed-pump drivers rated 15.6 MW at 5100 rpm for the German utility company STEAG. These LCI-supplied motors operate successfully since 1981 in a thermal power plant 24 hours/365 days without being disassembled for service. The drives initiated the industrial use of high-speed LCI drives and have many similar installations.
     
 
 

 © Siemens AG 2008 - Oil & Gas
Corporate Information / Privacy Policy / Terms of Use / Digital ID