|
Strip
geometry has for a long time included
not only width and thickness, but also
profile and flatness. To meet the
associated high requirements of the
market, the Siemens Profile and
Flatness Control (PFC) system builds on
sophisticated physical models. For
example, a roll temperature model
analyzes and considers the asymmetrical
conditions on the roll surface, while a
material flow model calculates the roll
pressure distribution across the length
and width of the roll gap as well as
the strip flatness after each stand.
Based on these data, the Siemens PFC
system not only makes sure that the
finished strip has the desired profile
or contour and the desired flatness.
The flatness between stands is also
taken into account in determining the
optimum settings of the actuators –
such as bending forces, CVC positions
and/or PairCross settings.
The Siemens PFC system that was used
first at the German EKO Stahl GmbH sets
standards with respect to the reliable
attainment of the desired strip
geometry.
|