siemens.com
Industry Sector
Home | Solutions and Services | News Center | Support | About Us
Site Map | Contact
 
Pulp & Paper
Cement
Marine Solutions
SIMAIN Industrial Maintenance
Industrial IT Solutions
Simulation & Testing
HMI & Industrial Communication
IT Enterprise
MES Solutions & IT Intralogistics
IT SW-Factory & Development
Electrical Power Solutions
Migration/ Modernization


 
 


Simulation & Testing - SIMIT

Testing and commissioning SIMATIC application software

SIMIT is the open platform for testing SIMATIC application software. Simulations of the process check that the SIMATIC automation environment is working properly. The result: greater certainty in planning and meeting of deadlines, reduction in costs and risk, significant improvements in terms of keeping to budget while at the same time reliably meeting the required quality standards.


The challenge

Three factors play a decisive role in implementing any system: meeting the agreed quality standards and remaining within cost and time limits. Whilst systems are becoming more individual, expectations of high levels of availability and efficiency are also rising. Modifications and enhancements now carry on well into the operational phase. The result is more complex projects, tighter timescales and more working at expensive times - either nights or weekends.

 

Our solution

SIMIT provides an extensive range of scalable products as a test platform for SIMATIC application software – from the simulation of a SIMATIC CPU with simple signals on the I/O level right through to interaction of the SIMATIC automation system with simulated and perhaps highly complex processes.
Integrated quality assurance
SIMIT enables the process simulation to be adjusted to your project – be it a standalone system or an entire plant. The advantage: in each phase of the project it is easy to check that the automation system is functioning correctly so that any errors can be detected and corrected at an early stage. Quality assurance is thus integrated directly into the projects.

Reliable technology and automation

SIMIT turns a virtual plant into reality: All the open- and closed-loop control functions in the plant, such as sequences, operator actions and the response to faults and operational errors, are reflected in SIMIT. Thus technicians and automation engineers share a common platform for objectively verifying the implementation of the automation task.

Commissioning in the office

SIMIT can be connected directly to the automation system, supplying it with accurate process data. This enables checks to be carried out from the office to confirm that the automation system is functioning correctly - just as if it were being commissioned on-site. Result: When the automation software is delivered to the installation site its quality status is known; this represents a huge stride in the direction of "switch-on commissioning".

No stresses on the plant's mechanical systems

SIMIT is based on plant simulations. The commissioning of the automation software therefore takes place without using the "real" plant – and thus without placing any unnecessary stresses on the mechanical components. Even malfunctions that cannot be tested for real in the plant due to the potentially serious risk to people and machinery can be reproduced in this way with SIMIT any number of times.

No disruption to operation

SIMIT enables software modifications to be performed and tested independently from the actual plant. A solution that has been developed in this way can then be installed very easily during a scheduled stoppage with no adverse effects on operation.

Good reasons for SIMIT

  • Early detection of errors in the automation software
  • Shorter project durations and lower project costs
  • No stress or risk to mechanical components
  • Less disruption of ongoing operation
  • ACoordinated process and automation system
 
 

 

 

 

  Contact

 

  FAQ, etc

 

© Siemens AG 2002-2009 - Industrial Technologies, Corporate Information | Privacy Policy | Terms of Use | Digital ID