Scope in project:
Mechanical process equipment of hot strip
mill
Capabilities and description:
China
National Erzhong Group Co.(Former The Second
Heavy Machinery Plant, hereinafter
abbreviated China Erzhong) is situated in
Deyang, a heavy industrial city on the west
plain of Sichuan province. It is the largest
heavy machine-building base and the
machinery localization base for the very
important technical equipment in China. It
is the important backbone enterprise which
are related with national economic lifeline
and state security. China Erzhong was built
up in 1958, and put into production in 1971.
It covers a total area of more than 2.61
million square meters. Now it possesses 8
branch works, 3 full capital subsidiary
companies and 6 holding subsidiary
companies, with the total assets about 4.7
billion yuan (RMB) (By the end of Dec.31 of
2004). There are 13,000 employees in this
company.
China Erzhong has a very strong capability
for the scientific researches. Its technical
centre is composed of Heavy Machinery Design
and Research Institute, Heavy Casting and
Forging Research Institute, Technology
Research Institute and the research
institutes of other specialities, which can
give energetic support to the development of
the new technique and the products.
China Erzhong
is equipped with modern equipment. It
possesses more than 6600 sets of various
kinds of manufacturing equipments. It has
the capability in smelting, foundry,
forging, heat-treatment, machining,
assembling, and the services after sales. So
it can produce 600 tons of super purity
liquid steel at one time, 400 tons of high
quality ingot, 400 tons of high quality
casting, 200 tons of high quality forging.
The machining capability for the heavy duty
complicated parts and components can be
performed as well. It also has the
transportation capability from 40t up to
400t by means of road, railway and water.
China Erzhong
has a perfect quality assurance system and
obtained ISO 9000 quality system
certification. It possesses advanced
inspection equipment and technique, such as
linear accelerator etc. which can guarantee
high quality products for the customers.
China Erzhong
has a very clear business concept. For more
than 40 years, China Erzhong always takes to
equip China with modern facilities, to
create the excellent products and services
to the world as its own task, and has
provided large amount of advanced world
levels complete sets of the production
lines, and high quality heavy castings and
forgings, die forgings to various industries
such as metallurgy, electric power, water
conservancy, chemical industry automobile,
aviation, aerospace, shipbuilding, nuclear
energy, transportation, mining, cement and
building material, agriculture and forestry,
etc. The products made by China Erzhong have
been supplied to all the country and the
world.
The customers
both at home and abroad are sincerely
welcomed to visit China Erzhong and to hold
business talks with us in order to create a
magnificent future.