|
|
 |
 |
 |
 |
| |
|
Project Example |
 |
|
Berlin-Tegel Airport
New communication system goes off the
blocks
Berlin-Tegel Airport has decommissioned
the telephone system it had been using
for over ten years and instead switched
to the
HiPath 4000 Real Time IP System
from Siemens. A soft migration strategy
is allowing new features to be
introduced but makes the whole process
far more secure. It also leaves the
door wide open to future advances. At
the same time, the new configuration
reduced costs considerably by reusing
certain existing modules and phones.
The first thing that interested the
management team was to map existing
features onto the new system as
smoothly as possible. But they also
wanted to set up a state-of-the-art
solution that would keep all their
options open for developments over the
next decade. Voice communication over
existing data networks on the basis of
the Internet Protocol – or
“communication over IP” (or CoIP) for
short – is one forward-looking topic
for which Ludwig Turba, Manager
Communication Systems at Berliner
Flughafen-Gesellschaft mbH, definitely
wants to be well-prepared. New network
management opportunities and the use of
unified messaging also had a bearing on
the decision, however – as, of course,
did the need to cut costs by minimizing
maintenance outlay and making the
system as failsafe as possible.
The airport’s telecoms experts scoured
the market and compared offers from a
number of vendors. In the end, however,
they opted for the migration solution
proposed by their existing supplier.
“The economic feasibility study showed
that we would still be able to use
around 30 to 40 percent of our existing
phones, as well as some of the modules
in the existing system,” Turba recalls.
In financial terms, that was a whole
lot better than moving over to a
completely new system. Moreover, this
solution would also let employees
continue to draw on existing expertise,
without the expense of extra training
measures.
During the migration project, 2300
ports on the old system were switched
over to the new one, 640 phones were
replaced by new optiPoint 500 models,
and one fax server and one digital
alarm and conference server were hooked
up to the new platform. The voice mail
system already in place was migrated to
a central unified messaging system
based on HiPath Xpressions. Now that
HiPath Manager is implemented,
centralized voice network management is
also available.
Some of the new features became
extremely popular almost before the
system as a whole was up and running.
One was the fact that callers are
listed on the phone, allowing callbacks
to be initiated at the push of a
button. Another was the ability to
check voice mailboxes from different
locations.
“For us, the intersite use of
applications will undoubtedly play a
major role in future,” says Ludwig
Turba, looking ahead. Unified messaging
applications and the ability to dial
phone numbers from within Microsoft
Outlook are important topics – not to
mention a full migration to CoIP.
|
 |
|
|
 |
|
|
|